text.skipToContent text.skipToNavigation
Price
Rating
10 Products found
  • TOP
    10 Products found

    Compare up to 4 items

    Please select up to 4 items to compare.
    OK

    Popular Questions

    What can I haul with a DR Versa-Trailer?

    We designed the DR Versa-Trailer for transporting all your biggest, heaviest, and bulkiest loads. Use it to haul everything from firewood, stones, and hay bales to mulch, leaves, brush, and gravel. The PRO 1000 model has an impressive 1,000-lb. capacity, while the top-of-the-line PRO XL2000 model can hold as much as 2,000 lbs. Both models can be easily reconfigured into a stake bed for hauling particularly long items, such as lumber or branches.

    What vehicles can I use to tow the DR Versa-Trailer?

    The DR Versa-Trailer can be towed behind any ATV, UTV, or vehicle that you don't mind using off-road. Both models feature a 2" ball hitch for towing.

    Reviews

    DR Versa-Trailer Reviews

    Exactly What I Have Been Looking For

    "I purchased the Versa Trailer and a 30XL chipper in July. I can hook both machines in tandem behind my 4-wheeler and go right to the tree I'm working on. I'm not sure why I waited so long to purchase one. I can now trim trees, chip them, and have mulch ready to go and can be dumped wherever I need without all the extra steps and labor. I also have a portable sawmill and the trailers ability to remove the dump bed and use as a logging trailer has made my life a whole lot easier. Thanks Again for a Great Product."

    - Matthew Campbell from CADDO MILLS, TX
    about the PRO 1000 Model

    Huge trailer

    "This is a monster of a trailer in an ATV size footprint. After years of operating various military equipment I have gotten used to having a tool for every job. This trailer is those tools in one. I live in the hills in Alaska and I can honestly say this trailer will go anywhere and haul almost anything. I wish it came with seats then I could use it for hay rides with my children. I love it ."

    - Schmoke220 from Alaska
    about the On the PRO 1000 Model

    This product exceeds my expectations

    "The Versa Trailer is the most utilized piece of machinery I use on my property. I like the tandem wheels as they walk over the dry creek bottom that ordinary single axle trailers would bounce over. I call it my moon walker! The dump truck feature has been used several times to unload gravel in a tight spot into my barn. Three tons of gravel on separate occasions were unloaded with ease. The swinging boom will be used to move 275 gallon water totes to and from the remote locations on my property to the water troughs. I pull it with ease with my 450 Kodiak Yamaha 4wheeler 4x4. Thank you for building a handy and useful trailer and putting it together was a snap, about 2 hrs. The instruction manual was spot on."

    - FAColdgame53 from Texas
    about the PRO 1000 Model

    Versa-Trailer 6ft tandem

    "Have enjoyed the use of my DR Trailer since I have got it. Makes clean up of my 6.5 acre yard much more easier and has added some fun to it. Wish I had bought one years ago. With all the trees and flower beds in our yard its been like having an extra set of hands. The dump bed makes unloading a breeze and take the bed off and we can haul all the big branches and fallen trees to the wood pile . My neighbors are always wanting to borrow it. Would buy another if anything ever happens to this one."

    - Larry57 from Tennessee
    about the PRO 1000 Model

    Excellent product

    "I've owned this for about a week and it has already paid for itself. It is a very high quality product and I certainly recommend."

    - Frank B. from Quakertown, PA
    about the PRO 1000 Model