text.skipToContent text.skipToNavigation
Price
Rating
2 Products found
  • TOP
    2 Products found

    Compare up to 4 items

    Please select up to 4 items to compare.
    OK

    Videos

    DR Edger

    DR Edger (1:38)



    Professional Edging

    Steel Bladed Edging

    A steel-bladed lawn edger is the professional choice for creating sharp, clean edges along walkways, garden borders, around trees, and anywhere else on your property where you want the precision of a well-defined cut. Professional edging defines these areas crisply and goes after the roots which, with most other edging techniques, are left unmolested and therefore need constant maintenance.


    For maximum stability a 4-wheel model like our DR PRO Lawn & Garden Edger will give you the best results. With four wheels on the ground you are free to concentrate on guiding the blade without any arduous lifting or exerting of downward pressure on the tool. You just steer the machine along and it does all the hard work. You just keep your line straight or guide it along the curve you desire.


    With a DR PRO Edger there is very little strain, so you can work for long periods of time without fatigue and without the sloppy cuts that inevitably come about with more labor-intensive methods.


    There are, of course—with any job—other ways to get the job done. The professional, knowing that time is money, will always opt for the most efficient method. As a homeowner you need to make a judgment, based on your own property, workload, and budget?about the best solution for you. Here are the most common alternatives to a professional edger:


    Manual Step Edgers.

    step edger

    A step edger, usually with a blade in the shape of a half-moon, is designed to be stepped on with one foot. Your weight sinks the blade into the earth to create a cut.


    PROS:

    • You can get good results if you are patient and willing to make a lot of cuts.
    • Wear and tear on your hands and feet. (You'll last longer with hard soled shoes and gloves, but even half an hour of this technique may wear you out.)
    • Inexpensive (the "cost" is in your labor).

    CONS:
    • Time consuming.
    • Only a small portion (the center of the half-moon) cuts to full depth. You need to maneuver the handle from side to side to widen the cut or make a new step-cut every 2-3 inches.


    String Trimmers.

    string trimmer

    Many string trimmers have heads that can be rotated 90° so you can run the string vertically instead of horizontally.


    PROS:

    • You can get good results if you don't mind doing it frequently.
    • Relatively inexpensive.

    CONS:
    • As with a manual wheeled edger, the cut tends to be superficial. If you don't cut deep enough to start severing roots (2-3") the edge will quickly grow over.
    • You need to be careful that the discharge doesn't flay your legs because, on many string trimmers, the protective shield is configured for trimming and doesn't do a good job of protecting the operator when used in edging mode.
    • With a string trimmer there is no point of contact with the ground to anchor your movement. As the operator's arms tire it's easy to wobble...and get a wobbly edge as a result.

    Manual Wheeled Edgers.

    wheel edger

    This style of edger consists of a rotary cutting blade attached to the end of a shaft with either one or two wheels. The idea is that you roll it along, pressing down on the shaft, and forcing the rotating blade to cut an edge.


    PROS:

    • You can get good results if you are willing to go over your edges several times.
    • Inexpensive (again the "cost" is in labor).

    CONS:
    • The cuts are usually too shallow to last. If you don't cut deep enough to start severing roots (2-3") the edge will quickly grow over.
    • If the cutting blade has a wide enough diameter to cut deeper, it is hard work to force it to the depth you want, and you may have to go over each cut several times.
    • Wear and tear on you. The pressure applied by pushing down on the shaft with one arm extended is something you'll feel in your shoulders and neck.


    Conclusion

    If edging is only a minor consideration on your property, you might be just fine with one of the more manual methods. However, the more edging you need to take care of, the more benefit you will get from going with a 4-wheel, steel-bladed edging tool like the DR PRO Lawn & Garden Edger. It not only creates the cleanest and longest-lasting edges, but it is also the fastest tool for the job!